Now at Mouser: Texas Instruments' Quad-Channel ADS54J64 Analog-to-Digital Converter Offers 1-GSPS Max Sample Rate
June 14, 2018 - Mouser Electronics, Inc., the industry's leading New Product Introduction (NPI) distributor with the widest selection of semiconductors and electronic components, is now stocking the quad-channel, 1 GSPS ADS54J64 analog-to-digital converter (ADC) from Texas Instruments (TI). The 14-bit ADS54J64 ADC offers high signal-to-noise ratio (SNR), wide bandwidth, and a maximum output sampling rate of 500 MSPS. Suitable for a variety of applications including telecommunications receivers and microwave receivers, the ADS54J64 ADC supports a high-speed JESD204B serial data interface, which simplifies connections to processors and offers data rates up to 10 Gbps with one lane per channel.
The TI ADS54J64 ADC, available from Mouser Electronics, provides uniform impedance across a wide frequency range through the use of an analog input buffer. The device offers low power consumption of just 2.5 W and provides an impressive spurious-free dynamic range (SFDR) over a wide input frequency range. The digital signal processing block supports up to a 200 MHz bandwidth and uses complex mixers followed by low-pass filters with decimate-by-2 and 4 options. The ADS54J64 ADC also offers support for multi-chip synchronization.
TI's ADS54J64 ADC is ideal for use in a range of equipment, including multi-carrier GSM base stations, telecommunications receivers, radar and antenna arrays, communications test equipment, microwave receivers, and digitizers. The ADS54J64 ADC can also be used in medical applications such as diagnostics and medical imaging.
To learn more, visit www.mouser.com/ti-ads54j64-adc.
With its broad product line and unsurpassed customer service, Mouser strives to empower innovation among design engineers and buyers by delivering advanced technologies. Mouser stocks the world's widest selection of the latest semiconductors and electronic components for the newest design projects. Mouser Electronics' website is continually updated and offers advanced search methods to help customers quickly locate inventory. Mouser.com also houses data sheets, supplier-specific reference designs, application notes, technical design information, and engineering tools.
About Mouser
Mouser Electronics, a Berkshire Hathaway company, is an award-winning, authorized semiconductor and electronic component distributor focused on rapid New Product Introductions from its manufacturing partners for electronic design engineers and buyers. The global distributor's website, Mouser.com, is available in multiple languages and currencies and features more than 5 million products from over 700 manufacturers. Mouser offers 23 support locations around the world to provide best-in-class customer service and ships globally to over 600,000 customers in more than 220 countries/territories from its 750,000 sq. ft. state-of-the-art facility south of Dallas, Texas. For more information, visit www.mouser.com.
Trademarks
Mouser and Mouser Electronics are registered trademarks of Mouser Electronics, Inc. All other products, logos, and company names mentioned herein may be trademarks of their respective owners.
Kevin Hess, Mouser Electronics
Senior Vice President of Marketing
(817) 804-3833
Kevin.Hess@mouser.com
Kelly DeGarmo, Mouser Electronics
Manager, Corporate Communications and Media Relations
(817) 804-7764
Kelly.DeGarmo@mouser.com